Part Number: TMS320F280049M
Other Parts Discussed in Thread: MOTORWARE, C2000WARE, DESIGNDRIVE, CONTROLSUITE
Hi, we have developed a family of motor controller products using F28027 and F28069 mcus and (heavily modified) MotorWare and are very intrigued by the F280049. However, I understand that although F280049M includes InstaSPIN functions, no official support is available yet.
Looking though the F280049 C2000Ware examples, it seems that porting our codebase from the MotorWare handle-based HAL/drivers to the new driverlib is not too difficult, however I am not yet convinced there is any point in doing so:
- The required InstaSPIN library and headers for F280049 are not released yet. Without them we could only modify our code to remove sensorless operation (i.e. FAST estimation) but even then we would need to reimplement some CTRL functions. Do I get this right?
- What is the schedule for official InstaSPIN support for F280049 by TI? Will it come as an Application SDK on top of C2000Ware? If yes, will it include support for F28027 and F28069 (although I don't see a driverlib for these)? That would be great, enabling a common code base for all InstaSPIN enebaled mcus. MotorWare HAL was unnecessarily separated for each Picollo line (separate but identical drivers etc), C2000 / driverlib seem to be in the right direction, will it support other Picollo lines (02x, 06x) in the future?
- Can TI at least release the required library and header files for F280049 so that we can use them with (ported) MotorWare?
Any info appreciated,
Giannis