Team,
My customer has the following question:
I have another question on the processor’s A/D, this time about the power supply pins. The datasheet says it would like VDDA to be between 3.14V and 3.47V. My 3.3V supply could possibly dip below this briefly (and possibly overshoot) when we transmit data on a MIL-STD-1553 bus. My 3.3VDDA is supplied from a ‘filtered’ 3.3VD (supply to VDDIO and such as well as everything else in the system). VREFHI is 2.5V. Do you know if these transients could affect the A/D conversions? Do you know if supplying VDDA with 2.8V or 3.0V would have any detrimental effects? I’m thinking of replacing the LC filter with an LDO with high PSRR/line regulation, but would like to supply it from the 3.3VD.
Regards,
Aaron