This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Interfacing with ADC Modules

Part Number: LAUNCHXL-F28379D


Hello Everyone

I'm Using LEM LV 25-P Voltage Transducer and LA 25-NP and current Transducer to measure AC Voltages and Currents Respectively. I Found that the ADCs of Launchxl F28379D has the range of 0 V to 3V according to the schematic provided in C2000 ware. Is that correct ?. If any reference designs are available for input signal conditioning for this kind of transducers (which gives a bipolar Output), Please guide me towards that. Thank you

with best regards,

Thilesh De Silva