Part Number: TMS320F28379D
Other Parts Discussed in Thread: AFE031
Tool/software: Code Composer Studio
Hi:
I have a problem in debugging the borad using MCU--TMS320F28379D made by myself. When testing, I tryed some code of TI's example device support works and they can debug with no errors. But the example code 'boostxl_afe031_f28379d_dacmode' got in trouble which works well in LAUNCHXL-F28379D.
The error shows as followed:
I looked help from the link bellow:

and found that the error happened in running program after successful loading, (I trird to locate the problem by steps: launch configuration,connetion,loading code and debug. )
The link point out this error and I Print Screen as the following picture shown marked by red line:
It says the application needs to be fixed. But I can not figure out how to solve the problem fix it because the code I used is the example code of TI and it works well in other LAUNCHXL-F28379D.
Besides that, the hardwared made by me doesn't include hardware reset part and I do want to ask if the error happen because of the unconnection in pin XRS_N?
Can anyone give me some advice?
Best regards,Ditny.