Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D, CONTROLSUITE
Tool/software: Code Composer Studio
I'm testing the LAUNCHXL-F28379D by using the example projects provided by texas instruments, the problem is that the PWM frequency is always half of the examples.. I have tried many examples in the controlsuite and also the examples provided in "http://processors.wiki.ti.com/index.php/C2000_One-Day_Workshop". The last one I tried in the the workshop "http://processors.wiki.ti.com/index.php/C2000_One-Day_Workshop" with the project named "Lab3_cpu01" was supposed to present a 2kHz PWM output... However, when measuring with the oscilloscope the output frequency is 1kHz...
I just bought this board and I'm wondering if the board is somehow deffective...
Can anyone please help me?