Part Number: TMS320F28075
Other Parts Discussed in Thread: UNIFLASH, , CCSTUDIO, POWERSUITE, SYSBIOS
Tool/software: Code Composer Studio
Hi,
I have the problem that my CCS (Version: 6.1.1.00022) fails to program the flash of _some_ of my 28075 devices (others work well). I use XDS560v2 LC and TI XDS100v3. The devices that CCS fails with can be programmed with Uniflash and XDS100v3 and afterwards debugged with CCS and XDS560v2 (no password lock etc.).
I get error messages like this:
C28xx_CPU1: Error during Flash programming (Flash algorithm returned error code). Operation cancelled.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: J:\workspace\firmware\c2000\scm_firmware\debug_flash\scm_firmware.out: Load failed.
Do you have any idea what the reason may be, or how to get more information to find it out?
Regards,
Frank