Part Number: DRV8301-69M-KIT
Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
Hi all,.
I'm using DRV8301-69M-KIT supplying with 40V DC.
The motor that i use is ACIM without nameplate. I only knows the supply voltage 12V and connection diagram Y.
I have tried lab 2a(MotorWare) but I have stucked in MOTOR ID proccess(cannot evaluate the rated flux).
Generally, the motor does not spin with proper 5.0 Hz that i set in the USER.H and I think it does not use the proper algorithm