Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D, C2000WARE
Tool/software: Code Composer Studio
Hello,
I use CCS7 and a Development Kit :LAUNCHXL-F28379D and i install C2000.
I want re-use a project. This project works. I just have an other PC with the same window and i make the installation of C2000 V3 et controlesuite.
When I want build, i have this errors:
error : cannot open source files :
#1965 cannot open source file "ti/targets/select.h" .ccsproject /Example_CPU1 line 87, external location: C:\ti\xdctools_3_50_04_43_core\packages\xdc\std.h C/C++ Problem
I don't find "select.h" anywhere.
This problems come after I add "xdctools_3_50_30_33 " because i had a error about std.h. (the projet was a broke link to xdctools_3_50_30_33 so i download and add) and after resolve on this forum an problem of conflict betwen headers.
Thank you in advance.
Best regards