Hi there,
My questions is with regards to the XCLKOUT signal when using a 150MHz external oscillator
1. Is the XCLKOUT signal continuous once stable at 150MHz.
2. How long does it take XCLKOUT signal to stabilise to 150MHz upon power up as I can see from the data sheet it goes through various transitions. The datasheet is not clear about this. Can you please explain in detail.
3. Can I use XCLKOUT signal to drive external logic like (DPRAM IP) inside a FPGA device without locking the logic out due to the various transitions of clock at power up.
Best regards,
Dhaivat