This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSDOCK28335: TMDSDOCK28335

Part Number: TMDSDOCK28335

Tool/software: Code Composer Studio

Hi,

Our goal is to control a single-phase converter using the ePWM of DSPF28335 with CCSV7 and Matlab 2017b.

We are starting with 2 basic test: 1) by injecting only sine signal into the ePWM. At the beginning, the output signal is not giving the attending result and the high frequency switching disappears after 2 or three hours as shown in Figure 1 and 2;

2) Test by generating a control signal using a percentage including in the ePWM (CMPA=7500 which corresponds to duty cycle of 50 % and switching frequency fs = 5kHz). The output signal remains constant even after 1 day of operation. See the Figure 3 and 4.