This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: about the Vloop of BLPFC

Other Parts Discussed in Thread: CONTROLSUITE

Tool/software: Code Composer Studio

When I use the Build3 to my BLPFC board 。

The output voltage reach to the 310V ,the TI program's PWM will shunt dowm 。

I think the output voltage is divided across three series resistors by 1M、1M and 22k,while the output voltage reach 310V ,this already over the VBUS_OVP_THRSHLD ((int32)((440.0/VBUS_FULL_RANGE)*4096*4096)) 

what can I do to solve this problem or what the TI do to solve this problem 

the SCH is from controlSUITE\development_kits\BLPFC_v1.0\Hardware
the software is from controlSUITE\development_kits\BLPFC_v1.0

  • 310V should not activate OVP. As you can see from the BridgelessPFC-Settings.h file the OVP threshold voltage (for Vout) is set to 440V. Also Vout sense resistors are R13(1M), R14(1M) and R15(13k). This means VBUS_FULL_RANGE (corresponding to 3.3V at the ADC input) is about 510V. So the per unit Vout reading, when OVP is activated should be 440/510 = 0.863.
    This kit is configured to output 400V. These settings are in BridgelessPFC-Settings.h and the related parameters are:

    #define VBUS_RATED_VOLTS (400.0)
    #define VBUS_OVP_THRSHLD ((int32)((440.0/VBUS_FULL_RANGE)*4096*4096))
    #define VBUS_TARGET ((int32)((VBUS_RATED_VOLTS/VBUS_FULL_RANGE)*4096*4096))

    Please review the User-Guide and run Build-1 and Build - 2 software to check the Vout reading using CCS RT Watch window. For example if your Vout is 310V then the per unit reading should be 310/510 = 0.607

    Shamim