Other Parts Discussed in Thread: C2000WARE
I am using a serial flash programmer to program (using UART) a TMS320F280049 controller on a custom PCB board. But there seems to be an error while loading the kernel.There seems to be an error called "error
with autobaud lock echoback".
The error screenshot is attached here.
I set the microcontroller in the SCI bootload mode.
- GPIO 32- set as high using a 10Kohm resistor to 3.3V.
- GPIO 24- set as low by grounding.
- GPIO 16 (SCIA_TX) connected to RX pin of the converter. The line is pulled up to 3.3V using a 10Kohm resistor.
- GPIO 17(SCIA_RX) connected to TX of the converter. The line is pulled up to 3.3V using a 10Kohm resistor