This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377D: How to set a GPIO to send a trip signal to force PWM low?

Part Number: TMS320F28377D

Tool/software: Code Composer Studio

Hi,

I am wondering if I can use a GPIO, for example GPIO119 to send a trip signal to the ePWMs, forcing it low?  If so, could you please review and correct the following code for me. I don't get PWM signals out, always low.

1. assign GPIO119 to INPUT1.

 EALLOW;
    InputXbarRegs.INPUT1SELECT = 119;
    GpioDataRegs.GPDDAT.bit.GPIO119 = 0;
 EDIS;

2.     initialize it in ePWM2
    EALLOW;
   EPwm2Regs.TZSEL.bit.OSHT1 = 1;  // Trip-zone 1 (TZ1) Select
    EPwm2Regs.TZEINT.bit.OST=1;
    EPwm2Regs.TZCTL.bit.TZA = 2;    // EPWM2A forces to low
    EPwm2Regs.TZCLR.bit.OST = 1;    // clear trip zone flags
    EDIS;
}

  • Wan,

    Give me sometime to look up some of the specific things you are using in your design and get back to you.
  • Please view this example,

    It should cover all you need. You must change the GPIO number to the one you require.

    //###########################################################################
    //
    // FILE:   epwm_trip_zone.c
    //
    // TITLE:  ePWM module using Trip-Zone submodule.
    //
    //! \addtogroup cpu01_example_list
    //! <h1> EPWM Trip Zone Module (epwm_trip_zone)</h1>
    //!
    //! This example configures ePWM1 and ePWM2 as follows
    //!  - ePWM1 has TZ1 as one shot trip source
    //!  - ePWM2 has TZ1 as cycle by cycle trip source
    //!
    //! Initially tie TZ1 high. During the test, monitor ePWM1 or ePWM2
    //! outputs on a scope. Pull TZ1 low to see the effect.
    //!
    //!  \b External \b Connections \n
    //!  - EPWM1A is on GPIO0
    //!  - EPWM2A is on GPIO2
    //!  - TZ1 is on GPIO12
    //!
    //! This example also makes use of the Input X-BAR. GPIO12 (the external
    //! trigger) is routed to the input X_BAR, from which it is routed to TZ1.
    //!
    //! The TZ-Event is defined such that EPWM1A will undergo a One-Shot Trip
    //! and EPWM2A will undergo a Cycle-By-Cycle Trip.
    //!
    //              _____________             __________________
    //              |           |             |                |
    //  GPIO12 -----| I/P X-BAR |-----TZ1-----| ePWM TZ Module |-----TZ-Event
    //              |___________|             |________________|
    //
    //
    //
    //###########################################################################
    // $TI Release: F2837xD Support Library v3.01.00.00 $
    // $Release Date: Mon May 22 15:43:40 CDT 2017 $
    // $Copyright:
    // Copyright (C) 2013-2017 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without 
    // modification, are permitted provided that the following conditions 
    // are met:
    // 
    //   Redistributions of source code must retain the above copyright 
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the 
    //   documentation and/or other materials provided with the   
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################
    
    //
    // Included Files
    //
    #include "F28x_Project.h"
    
    //
    // Defines
    //
    #define EXTTrig     // Leave Uncommented for Testing with External Trigger.
                        // Comment for Testing with ePWM Trigger.
    
    //
    // Globals
    //
    Uint32  EPwm1TZIntCount;
    Uint32  EPwm2TZIntCount;
    
    //
    // Function Prototypes
    //
    void InitEPwm1Example(void);
    void InitEPwm2Example(void);
    void InitTzGpio(void);
    __interrupt void epwm1_tzint_isr(void);
    __interrupt void epwm2_tzint_isr(void);
    void InitEPwmGpio_TZ(void);
    
    //
    // Main
    //
    void main(void)
    {
    //
    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the F2837xD_SysCtrl.c file.
    //
        InitSysCtrl();
    
    //
    // Step 2. Initialize GPIO:
    // This example function is found in the F2837xD_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    //
    //    InitGpio();
    
    //
    // enable PWM1, and PWM2
    //
        EALLOW;
        CpuSysRegs.PCLKCR2.bit.EPWM1=1;
        CpuSysRegs.PCLKCR2.bit.EPWM2=1;
        EDIS;
    
    //
    // For this case just init GPIO pins for ePWM1, ePWM2, ePWM3
    //
        InitEPwmGpio_TZ();
        InitTzGpio();
    
    //
    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
    //
        DINT;
    
    //
    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the F2837xD_PieCtrl.c file.
    //
        InitPieCtrl();
    
    //
    // Disable CPU interrupts and clear all CPU interrupt flags:
    //
        IER = 0x0000;
        IFR = 0x0000;
    
    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in F2837xD_DefaultIsr.c.
    // This function is found in F2837xD_PieVect.c.
    //
        InitPieVectTable();
    
    //
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    //
        EALLOW; // This is needed to write to EALLOW protected registers
        PieVectTable.EPWM1_TZ_INT = &epwm1_tzint_isr;
        PieVectTable.EPWM2_TZ_INT = &epwm2_tzint_isr;
        EDIS;   // This is needed to disable write to EALLOW protected registers
    
    //
    // Step 4. Initialize the Device Peripherals:
    //
        EALLOW;
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =0;
        EDIS;
    
        InitEPwm1Example();
        InitEPwm2Example();
    
        EALLOW;
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =1;
        EDIS;
    
    //
    // Step 5. User specific code, enable interrupts:
    //
        EPwm1TZIntCount = 0;
        EPwm2TZIntCount = 0;
    
    //
    // Enable CPU INT2 which is connected to EPWM1-3 INT:
    //
        IER |= M_INT2;
    
    //
    // Enable EPWM INTn in the PIE: Group 3 interrupt 1-3
    //
        PieCtrlRegs.PIEIER2.bit.INTx1 = 1;
        PieCtrlRegs.PIEIER2.bit.INTx2 = 1;
    
    //
    // Enable global Interrupts and higher priority real-time debug events:
    //
        EINT;  // Enable Global interrupt INTM
        ERTM;  // Enable Global realtime interrupt DBGM
    
    //
    // Step 6. IDLE loop. Just sit and loop forever (optional):
    //
        for(;;)
        {
            asm ("  NOP");
        }
    }
    
    //
    // epwm1_tzint_isr - EPWM1 TZ ISR
    //
    __interrupt void epwm1_tzint_isr(void)
    {
        EPwm1TZIntCount++;
    
        //
        // To Re-enable the OST Interrupt, do the following:
        // EALLOW;
        // EPwm1Regs.TZCLR.bit.OST = 1;
        // EPwm1Regs.TZCLR.bit.INT = 1;
        // EDIS;
        //
    
        //
        // Acknowledge this interrupt to receive more interrupts from group 2
        //
        PieCtrlRegs.PIEACK.all = PIEACK_GROUP2;
    }
    
    //
    // epwm2_tzint_isr - EPWM2 TZ ISR
    //
    __interrupt void epwm2_tzint_isr(void)
    {
        GpioDataRegs.GPATOGGLE.bit.GPIO11 = 1;
    
        EPwm2TZIntCount++;
    
        //
        // Clear the flags - we will continue to take
        // this interrupt until the TZ pin goes high
        //
        EALLOW;
        EPwm2Regs.TZCLR.bit.CBC = 1;
        EPwm2Regs.TZCLR.bit.INT = 1;
        EDIS;
    
        //
        // Acknowledge this interrupt to receive more interrupts from group 2
        //
        PieCtrlRegs.PIEACK.all = PIEACK_GROUP2;
    }
    
    //
    // InitEPwm1Example - Initialize EPWM1 configuration
    //
    void InitEPwm1Example()
    {
        //
        // Enable TZ1 as one shot trip sources
        //
        EALLOW;
        EPwm1Regs.TZSEL.bit.OSHT1 = 1;
    
        //
        // Set TZA
        //
        EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_HI;
    
        //
        // Enable TZ interrupt
        //
        EPwm1Regs.TZEINT.bit.OST = 1;
        EDIS;
    
        EPwm1Regs.TBPRD = 12000;                        // Set timer period
        EPwm1Regs.TBPHS.bit.TBPHS = 0x0000;             // Phase is 0
        EPwm1Regs.TBCTR = 0x0000;                       // Clear counter
    
        //
        // Setup TBCLK
        //
        EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
        EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;        // Disable phase loading
        EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV4;       // Clock ratio to SYSCLKOUT
        EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV4;
    
        EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;    // Load registers every ZERO
        EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
    
        //
        // Setup compare
        //
        EPwm1Regs.CMPA.bit.CMPA = 6000;
    
        //
        // Set actions
        //
        EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;             // Set PWM1A on CAU
        EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR;           // Clear PWM1A on CAD
    }
    
    //
    // InitEPwm2Example - Initialize EPWM2 configuration
    //
    void InitEPwm2Example()
    {
        //
        // Enable TZ1 as one cycle-by-cycle trip sources
        //
        EALLOW;
        EPwm2Regs.TZSEL.bit.CBC1 = 1;
    
        //
        // Set TZA
        //
        EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_HI;
    
        //
        // Enable TZ interrupt
        //
        EPwm2Regs.TZEINT.bit.CBC = 1;
        EDIS;
    
        EPwm2Regs.TBPRD = 6000;                       // Set timer period
        EPwm2Regs.TBPHS.bit.TBPHS = 0x0000;           // Phase is 0
        EPwm2Regs.TBCTR = 0x0000;                     // Clear counter
    
        //
        // Setup TBCLK
        //
        EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
        EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE;        // Disable phase loading
        EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV4;       // Clock ratio to SYSCLKOUT
        EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV4;          // Slow just to observe on
                                                       // the scope.
    
        //
        // Setup compare
        //
        EPwm2Regs.CMPA.bit.CMPA = 3000;
    
        //
        // Set actions
        //
        EPwm2Regs.AQCTLA.bit.CAU = AQ_SET;             // Set PWM2A on CAU
        EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR;           // Clear PWM2A on CAD
    }
    
    //
    // InitTzGpio - Initialize TZ GPIOs
    //
    void InitTzGpio(void)
    {
        //
        // For External Trigger, GPIO12 as the trigger for TripZone
        //
        GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0;    // Enable pull-up on GPIO12 (TZ1)
    
        GpioCtrlRegs.GPAQSEL1.bit.GPIO12 = 3;  // Asynch input GPIO12 (TZ1)
    
        EALLOW;
        InputXbarRegs.INPUT1SELECT = 12;
        EDIS;
    
        //
        // For monitoring when the TZ Interrupt has been entered
        //
        EALLOW;
        GpioCtrlRegs.GPAPUD.bit.GPIO11 = 1;    // Disable pull-up on GPIO0 (EPWM1A)
        GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 0;   // Configure GPIO0 as EPWM1A
        GpioCtrlRegs.GPADIR.bit.GPIO11 = 1;
        EDIS;
    }
    
    //
    // InitEPwmGpio_TZ - Initialize EPWM1A and EPWM2A GPIOs
    //
    void InitEPwmGpio_TZ(void)
    {
        EALLOW;
        GpioCtrlRegs.GPAPUD.bit.GPIO0 = 1;    // Disable pull-up on GPIO0 (EPWM1A)
        GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1;   // Configure GPIO0 as EPWM1A
        GpioCtrlRegs.GPAPUD.bit.GPIO2 = 1;    // Disable pull-up on GPIO2 (EPWM2A)
        GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1;   // Configure GPIO2 as EPWM2A
        EDIS;
    }
    
    //
    // End of file
    //
    

  • Thank you, Nima.

    It can work for One-Shot Trip. However the trip flag will automatically be cleared when the GPIO is low.

    I wish once the system is tripped, the trip will stand and only be cleared manually. So is there any other register that needs setting?

  • Here is the snapshot for the Tripzone Flag Registers. TZFLG and TZOSTFLG always stay zero whenever the trip is triggered or not. Once tripped, OST bit should be written to 1, is that right?

  • Can you show me what actions you are taking in your interrupt routine?
    Also are you entering the interrupt routine successfully?
  • Wan,
    According to the TRM,
    "Additionally, when a one-shot trip event occurs, the one-shot trip event flag (TZFLG[OST]) is set and a
    EPWMx_TZINT interrupt is generated if it is enabled in the TZEINT register and PIE peripheral. A
    corresponding flag for the event that caused the OST event is also set in register TZOSTFLG. The
    one-shot trip condition must be cleared manually by writing to the TZCLR[OST] bit. If desired,
    TZOSTFLG register bit should be cleared by manually writing to the corresponding bit in the
    TZOSTCLR register."

    These registers must be cleared manually. Please review your code for places where you could have cleared the flags using TZCLR and TZOSTCLR.