Other Parts Discussed in Thread: DRV8301
Good day,
I got a fault when stopping my DRV8301 HC kit. I modified the code to work as a H-bridge and Switch to power a Brushed DC motor with a field winding.
Once I enable the system the DRV faults instantly and makes a high pitch buzzing sound. It was running fine so I am not sure why it fault. The is not visual damage to the board or burning smell. I tried resetting and reprogramming.
I assume the DRV is the problem but I want to make sure, also how would I go about replacing it. Also If the problem could be from the transistor side?