Part Number: TMS320F28335
Tool/software: Code Composer Studio
Respected Sir,
I connected the probe ,after that I have tried the Target confign i.e.[probe=TI XDS100v2 USB Debug probe] and controller is TMS320F28335 is selected.But test connection is failed.Not able to dump the program.whilie dumping the program following message come,how to resolve the above problem.
Error msg as follows:
Error connecting to the target:
(Error -1015 @ 0x0)
Device is not responding to the request. Device may be locked, or the debug probe connection may be unreliable. Unlock the device if possible (e.g. use wait in reset mode, and power-cycle the board). If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 7.0.100.1)