Part Number: TMDXIDDK379D
Hi,
I have purchased the C2000 Dev Kit bundle for driving a 3 Phase motor (https://store.ti.com/TMDXIDDK379D-MTR-BNDL.aspx
Sensored Field Oriented Control of 3 - Phase Permanent Magnet Synchronous Motors using F2837x" page 32 is guiding me to Run the motor and adjust the PI values for IdRef and IqRef. No matter what I am adjusting, nothing changes. Is there any information/videos of someone going through the kit step by step and getting it to run (Other than the manual I currently have). Could any one provide any additional guidance?
I have attached an image of the code running in LEVEL3 build. You can see that the EnabledFlag is 1, the MotorRun is 1 and I have set the IqRef to 0.05 (as per manual) and SpeedRef to 0.1 (I had it set to 0.3 as per manual).
The two graphs on the right side are pi_iq.Fbk and pi_id.Fbk respectively. I can change the pi_iq.Kp or Ki values but the graphs never change. In addition, with these default values, the graphs look a bit strange too.
Any advice would be greatly appreciated.