This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2812: power sequencing issue

Part Number: TMS320F2812

Hi,

Base on F2812 data sheet,  section 6.8 Power Sequencing Requirements option2,

First 3.3V on, then 1.9V ramp,

Other condition: 1.8 V or 1.9 V (V DD /V DD1 ) should not reach 0.3 V until V DDIO has reached 2.5 V.

Power ramp up as below picture, CS pin will have a low state to access FARM when power ramp up.

but if 1.9V and 3.3V ramp up together as below picture , CS pin also ramp up high level  when power ramp up.

It did not have low state to access FARM incorrectly.

Is it possible that DSP power-on fail  when 1.9V and 3.3V ramp up together ?

thanks,

best regards,

Simen