Other Parts Discussed in Thread: TIDA-01407, TIDM-BIDIR-400-12
Dears,
My company is doing OBC design and DCDC design. I am very interested in TI product.
Is there any reference design for this case?
1st Case:
High Frequency Phase-Shift Full-Bridge:
Frequency around 200K.
Input:750V
output:14V or 24V
2-3KW
2nd Case:
Bi-Directional DC-DC Design
35V for one side 750V for another.
3kW
Any reference design for this case? I find some reference like TIDA-01407 and TIDM-BIDIR-400-12.
Is that OK to enhance the input the voltage. Any drive, controller suggestion?
Many thanks