This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377S: SPI PROBLEM

Part Number: TMS320F28377S


Tool/software: Code Composer Studio

Hi

I am trying to connect through the spi with external flash memory (MICROCHIP SST26VF064B) and I have a problem. When I m trying read ID of memory I do not get what I should. Could anone help me with this problem?

#include "F28x_Project.h"

void delay_loop(void);
void spi_xmit(Uint16 a);
void spi_fifo_init(void);
void spi_init(void);
void error(void);

void main(void)
{
   Uint16 sdata;  // send data
   Uint16 rdata;  // received data

   InitSysCtrl();

   GpioDataRegs.GPBCLEAR.bit.GPIO63 = 1;

   InitSpiaGpio();
   InitSpi();
   DINT;

   InitPieCtrl();

   IER = 0x0000;
   IFR = 0x0000;

   InitPieVectTable();



//   sdata = 0x009F;

   for(;;)
   {
       GpioDataRegs.GPCCLEAR.bit.GPIO64 = 1;

        spi_xmit(0x9F);
        rdata = SpiaRegs.SPIRXBUF;


        GpioDataRegs.GPCSET.bit.GPIO64 = 1;



   }
}

void error(void)
{
    asm("     ESTOP0");     // Test failed!! Stop!
    for (;;);
}

void spi_xmit(Uint16 a)
{
    SpiaRegs.SPITXBUF = a;
}
//###########################################################################
//
// FILE:   F2837xS_Spi.c
//
// TITLE:  F2837xS SPI Initialization & Support Functions.
//
//###########################################################################
// $TI Release: F2837xS Support Library v3.04.00.00 $
// $Release Date: Sun Mar 25 13:27:27 CDT 2018 $
// $Copyright:
// Copyright (C) 2014-2018 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
#include "F2837xS_device.h"
#include "F2837xS_Examples.h"

//
// Calculate BRR: 7-bit baud rate register value
// SPI CLK freq = 500 kHz
// LSPCLK freq  = CPU freq / 4  (by default)
// BRR          = (LSPCLK freq / SPI CLK freq) - 1
//
#if CPU_FRQ_200MHZ
#define SPI_BRR        ((200E6 / 4) / 500E3) - 1
#endif

#if CPU_FRQ_150MHZ
#define SPI_BRR        ((150E6 / 4) / 500E3) - 1
#endif

#if CPU_FRQ_120MHZ
#define SPI_BRR        ((120E6 / 4) / 500E3) - 1
#endif

//
// InitSPI - This function initializes the SPI to a known state
//
void InitSpi(void)
{
    // Initialize SPI-A

    // Set reset low before configuration changes
    // Clock polarity (0 == rising, 1 == falling)
    // 16-bit character
    // Enable loop-back
    SpiaRegs.SPICCR.bit.SPISWRESET = 0;
    SpiaRegs.SPICCR.bit.CLKPOLARITY = 0;
    SpiaRegs.SPICCR.bit.SPICHAR = (7);
    SpiaRegs.SPICCR.bit.SPILBK = 0;

    // Enable master (0 == slave, 1 == master)
    // Enable transmission (Talk)
    // Clock phase (0 == normal, 1 == delayed)
    // SPI interrupts are disabled
    SpiaRegs.SPICTL.bit.MASTER_SLAVE = 1;
    SpiaRegs.SPICTL.bit.TALK = 1;
    SpiaRegs.SPICTL.bit.CLK_PHASE = 0;
    SpiaRegs.SPICTL.bit.SPIINTENA = 0;

    // Set the baud rate
    SpiaRegs.SPIBRR.bit.SPI_BIT_RATE = SPI_BRR;

    // Set FREE bit
    // Halting on a breakpoint will not halt the SPI
    SpiaRegs.SPIPRI.bit.FREE = 1;

    // Release the SPI from reset
    SpiaRegs.SPICCR.bit.SPISWRESET = 1;
}

//
// InitSpiGpio - This function initializes GPIO pins to function as SPI pins.
//               Each GPIO pin can be configured as a GPIO pin or up to 3
//               different peripheral functional pins. By default all pins come
//               up as GPIO inputs after reset.
//
//               Caution:
//               For each SPI peripheral
//               Only one GPIO pin should be enabled for SPISOMO operation.
//               Only one GPIO pin should be enabled for SPISOMI operation.
//               Only one GPIO pin should be enabled for SPICLK  operation.
//               Only one GPIO pin should be enabled for SPISTE  operation.
//               Comment out other unwanted lines.
//
void InitSpiGpio()
{
   InitSpiaGpio();
}

//
// InitSpiaGpio - Initialize SPIA GPIOs
//
void InitSpiaGpio()
{
   EALLOW;

    //
    // Enable internal pull-up for the selected pins
    //
    // Pull-ups can be enabled or disabled by the user.
    // This will enable the pullups for the specified pins.
    // Comment out other unwanted lines.
    //
    GpioCtrlRegs.GPBPUD.bit.GPIO58 = 0;  // Enable pull-up on GPIO16 (SPISIMOA)
    GpioCtrlRegs.GPBPUD.bit.GPIO59 = 0;  // Enable pull-up on GPIO17 (SPISOMIA)
    GpioCtrlRegs.GPBPUD.bit.GPIO60 = 0;  // Enable pull-up on GPIO18 (SPICLKA)


    //
    // Set qualification for selected pins to asynch only
    //

    // Comment out other unwanted lines.
    //
    GpioCtrlRegs.GPBQSEL2.bit.GPIO58 = 3; // Asynch input GPIO16 (SPISIMOA)
    GpioCtrlRegs.GPBQSEL2.bit.GPIO59 = 3; // Asynch input GPIO17 (SPISOMIA)
    GpioCtrlRegs.GPBQSEL2.bit.GPIO60 = 3; // Asynch input GPIO18 (SPICLKA)


    //
    //Configure SPI-A pins using GPIO regs
    //
    // This specifies which of the possible GPIO pins will be SPI functional
    // pins.
    // Comment out other unwanted lines.
    //
    GpioCtrlRegs.GPBMUX2.bit.GPIO58 = 3; // Configure GPIO16 as SPISIMOA
    GpioCtrlRegs.GPBMUX2.bit.GPIO59 = 3; // Configure GPIO17 as SPISOMIA
    GpioCtrlRegs.GPBMUX2.bit.GPIO60 = 3; // Configure GPIO18 as SPICLKA

    GpioCtrlRegs.GPBGMUX2.bit.GPIO58 = 3; // Configure GPIO16 as SPISIMOA
    GpioCtrlRegs.GPBGMUX2.bit.GPIO59 = 3; // Configure GPIO17 as SPISOMIA
    GpioCtrlRegs.GPBGMUX2.bit.GPIO60 = 3; // Configure GPIO18 as SPICLKA


    GpioCtrlRegs.GPCPUD.bit.GPIO64 = 0;   // Enable pull-up on GPIO58 (SPISTEA)
    GpioCtrlRegs.GPCMUX1.bit.GPIO64 = 0;    // 0=GPIO, 1=MCLKRA, 2=SCITXDB, 3=EPWM7A
    GpioCtrlRegs.GPCDIR.bit.GPIO64 = 1;     // 1=OUTput, 0=INput
//    GpioDataRegs.GPCSET.bit.GPIO64 = 1;     // uncomment if --> Set High initially

    GpioCtrlRegs.GPBPUD.bit.GPIO63 = 0;   // Enable pull-up on GPIO58 (WP)
    GpioCtrlRegs.GPBMUX2.bit.GPIO63 = 0;    // 0=GPIO, 1=MCLKRA, 2=SCITXDB, 3=EPWM7A
    GpioCtrlRegs.GPBDIR.bit.GPIO63 = 1;     // 1=OUTput, 0=INput
 //   GpioDataRegs.GPBSET.bit.GPIO63 = 1;     // uncomment if --> Set High initially

    EDIS;
}

//
// End of file
//

Best regards

Szymon

  • Hi Szymon,

    - Can you tell us what data you are expecting to receive and what data you are actually receiving?

    - What frequency is your SPI communication running at?

    - Have you verified the clock and phase settings programmed on the C28x match those specified in the external memory's datasheet?

    Regards,

    Kris

  • Hi Kris

    I should receive BFH 26H 43H.  My freq is 500kHz. Yes I verified clock and phase settings. I attach corrected code.

    #include "F28x_Project.h"
    
    void delay1_loop(void);
    void spi_xmit(Uint16 a);
    void spi_fifo_init(void);
    void error(void);
    void InitMySpi(void);
    void InitSpiGpioMy();
    void main(void)
    {
       Uint16 sdata;  // send data
       Uint16 rdata;  // received data
    
       InitSysCtrl();
    
       DINT;
    
       InitSpiGpioMy();
    
       InitPieCtrl();
    
       IER = 0x0000;
       IFR = 0x0000;
    
       InitPieVectTable();
    
       InitMySpi();
       spi_fifo_init();
    
    //   sdata = 0x009F;
       for(;;)
       {
            spi_xmit(0x009F); //transmija
            delay1_loop();
            while(SpiaRegs.SPIFFRX.bit.RXFFST !=1) { }
    
            rdata = SpiaRegs.SPIRXBUF; //odczyt
    
       }
    }
    
    
    void delay1_loop() //delay
    {
        long i;
        for (i = 0; i < 1000000; i++) {}
    }
    
    
    void error(void)
    {
        asm("     ESTOP0");
        for (;;);
    }
    
    
    void spi_xmit(Uint16 a) //transmisja
    {
        SpiaRegs.SPITXBUF = a;
    }
    
    
    void spi_fifo_init()
    {
    
        SpiaRegs.SPIFFTX.all = 0xE040;
        SpiaRegs.SPIFFRX.all = 0x2044;
        SpiaRegs.SPIFFCT.all = 0x0;
    }
    
    void InitMySpi(void)
    {
    
        SpiaRegs.SPICCR.bit.SPISWRESET = 0;
        SpiaRegs.SPICCR.bit.CLKPOLARITY = 0;
        SpiaRegs.SPICCR.bit.SPICHAR = (16-1);
        SpiaRegs.SPICCR.bit.SPILBK = 0;
    
    
        SpiaRegs.SPICTL.bit.MASTER_SLAVE = 1;
        SpiaRegs.SPICTL.bit.TALK = 1;
        SpiaRegs.SPICTL.bit.CLK_PHASE = 0;
        SpiaRegs.SPICTL.bit.SPIINTENA = 0;
    
        // Set the baud rate
        SpiaRegs.SPIBRR.bit.SPI_BIT_RATE = 99;
    
    
        SpiaRegs.SPIPRI.bit.FREE = 1;
    
        SpiaRegs.SPICCR.bit.SPISWRESET = 1;
    }
    
    void InitSpiGpioMy()
    {
       EALLOW;
    
    
        GpioCtrlRegs.GPBPUD.bit.GPIO58 = 0;  // Enable pull-up on GPIO16 (SPISIMOA)
        GpioCtrlRegs.GPBPUD.bit.GPIO59 = 0;  // Enable pull-up on GPIO17 (SPISOMIA)
        GpioCtrlRegs.GPBPUD.bit.GPIO60 = 0;  // Enable pull-up on GPIO18 (SPICLKA)
        GpioCtrlRegs.GPCPUD.bit.GPIO72 = 0;  // Enable pull-up on GPIO19 (SPISTEA)
    
        GpioCtrlRegs.GPBQSEL2.bit.GPIO58 = 3; // Asynch input GPIO16 (SPISIMOA)
        GpioCtrlRegs.GPBQSEL2.bit.GPIO59 = 3; // Asynch input GPIO17 (SPISOMIA)
        GpioCtrlRegs.GPBQSEL2.bit.GPIO60 = 3; // Asynch input GPIO18 (SPICLKA)
        GpioCtrlRegs.GPCQSEL1.bit.GPIO72 = 3; // Asynch input GPIO19 (SPISTEA)
    
        GpioCtrlRegs.GPBMUX2.bit.GPIO58 = 3; // Configure GPIO16 as SPISIMOA
        GpioCtrlRegs.GPBMUX2.bit.GPIO59 = 3; // Configure GPIO17 as SPISOMIA
        GpioCtrlRegs.GPBMUX2.bit.GPIO60 = 3; // Configure GPIO18 as SPICLKA
        GpioCtrlRegs.GPCMUX1.bit.GPIO72 = 3; // Configure GPIO19 as SPISTEA
    
        GpioCtrlRegs.GPBGMUX2.bit.GPIO58 = 3; // Configure GPIO16 as SPISIMOA
        GpioCtrlRegs.GPBGMUX2.bit.GPIO59 = 3; // Configure GPIO17 as SPISOMIA
        GpioCtrlRegs.GPBGMUX2.bit.GPIO60 = 3; // Configure GPIO18 as SPICLKA
        GpioCtrlRegs.GPCGMUX1.bit.GPIO72 = 3; // Configure GPIO19 as SPISTEA
    
        EDIS;
    }
    
    

    Best regards 

    Szymon

  • Hi Szymon,

    What is the data that you are actually receiving? I would like to compare it to the expected data to see if there is a bit shift or other discernible pattern.

    Regards,
    Kris
  • Hi,

    I received 0xFFFF

    Best regards 

    Szymon

  • Hi Szymon,

    This sounds like either the other device is not transmitting or the RX GPIO is not configured properly on the mux.

    Can you confirm that you are using GPIOs 58/59/60/72 for your SPI connection? GPIO72's SPISTEC is actually for a different SPI module than the other signals. The device has multiple SPIs. All of your other signals are for SPI-A so the signal you would want to use is SPISTE"A". What is likely happening is that the slave transmit enable isn't being set low to allow the slave to transmit. Therefore, you are receiving all '1's because your SOMI pin is pulled high.

    Regards,
    Kris
  • Hi 

    I changed configuration but I still not receive correct value. I checked the waves of signals on the oscilloscope. For MOSI, CLK and SPISTE"A" singlas, waves are corrected. As you wrote SPISTE "A" changes state from 0 to 1 when the Master start transmit.

     On MISO signal I always have high.

    #include "F28x_Project.h"
    
    void delay1_loop(void);
    void spi_xmit(Uint16 a);
    void spi_fifo_init(void);
    void error(void);
    void InitMySpi(void);
    void InitSpiGpioMy();
    void main(void)
    {
       Uint16 sdata;  // send data
       Uint16 rdata;  // received data
    
       InitSysCtrl();
    
       DINT;
    
       InitSpiGpioMy();
    
       InitPieCtrl();
    
       IER = 0x0000;
       IFR = 0x0000;
    
       InitPieVectTable();
    
       InitMySpi();
       spi_fifo_init();
    
    //   sdata = 0x009F;
       for(;;)
       {
            spi_xmit(0x009F); //transmija
            delay1_loop();
            while(SpiaRegs.SPIFFRX.bit.RXFFST !=1) { }
    
            rdata = SpiaRegs.SPIRXBUF; //odczyt
    
       }
    }
    
    
    void delay1_loop() //delay
    {
        long i;
        for (i = 0; i < 1000000; i++) {}
    }
    
    
    void error(void)
    {
        asm("     ESTOP0");
        for (;;);
    }
    
    
    void spi_xmit(Uint16 a) //transmisja
    {
        SpiaRegs.SPITXBUF = a;
    }
    
    
    void spi_fifo_init()
    {
    
        SpiaRegs.SPIFFTX.all = 0xE040;
        SpiaRegs.SPIFFRX.all = 0x2044;
        SpiaRegs.SPIFFCT.all = 0x0;
    }
    
    void InitMySpi(void)
    {
    
        SpiaRegs.SPICCR.bit.SPISWRESET = 0;
        SpiaRegs.SPICCR.bit.CLKPOLARITY = 0;
        SpiaRegs.SPICCR.bit.SPICHAR = (16-1);
        SpiaRegs.SPICCR.bit.SPILBK = 0;
    
    
        SpiaRegs.SPICTL.bit.MASTER_SLAVE = 1;
        SpiaRegs.SPICTL.bit.TALK = 1;
        SpiaRegs.SPICTL.bit.CLK_PHASE = 0;
        SpiaRegs.SPICTL.bit.SPIINTENA = 0;
    
        // Set the baud rate
        SpiaRegs.SPIBRR.bit.SPI_BIT_RATE = 99;
    
    
        SpiaRegs.SPIPRI.bit.FREE = 1;
    
        SpiaRegs.SPICCR.bit.SPISWRESET = 1;
    }
    
    void InitSpiGpioMy()
    {
       EALLOW;
    
    
        GpioCtrlRegs.GPAPUD.bit.GPIO16 = 0;  // Enable pull-up on GPIO16 (SPISIMOA)
        GpioCtrlRegs.GPAPUD.bit.GPIO17 = 0;  // Enable pull-up on GPIO17 (SPISOMIA)
        GpioCtrlRegs.GPAPUD.bit.GPIO18 = 0;  // Enable pull-up on GPIO18 (SPICLKA)
        GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0;  // Enable pull-up on GPIO19 (SPISTEA)
    
        GpioCtrlRegs.GPAQSEL2.bit.GPIO16 = 3; // Asynch input GPIO16 (SPISIMOA)
        GpioCtrlRegs.GPAQSEL2.bit.GPIO17 = 3; // Asynch input GPIO17 (SPISOMIA)
        GpioCtrlRegs.GPAQSEL2.bit.GPIO18 = 3; // Asynch input GPIO18 (SPICLKA)
        GpioCtrlRegs.GPAQSEL2.bit.GPIO19 = 3; // Asynch input GPIO19 (SPISTEA)
    
        GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 1; // Configure GPIO16 as SPISIMOA
        GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 1; // Configure GPIO17 as SPISOMIA
        GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 1; // Configure GPIO18 as SPICLKA
        GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 1; // Configure GPIO19 as SPISTEA
    
        EDIS;
    }

    Best regards

    Szymon

     
  • Hi Szymon,

    I just want to confirm, the SPISTE should be LOW while the master is transmitting. Can you confirm that is the case? If so, it seems the TI device is functioning as programmed. I would recommend reviewing the Microchip datasheet further to ensure you are communicating with the correct pins and have the communications configured correctly.

    Regards,

    Kris