I posted below in the wrong forum. Not sure if it matters, but I'd like to post it again in the 320C2000 forum.
====================================================
Hello Everyone,
My question is very simple. What's the effective (max) range/distance for SPI communication between 2 2812 processors? The processore clock speed is 120 MHz, and the SPI bus is running at 7.5MHz.
I know this can be a loaded question, as there's no standard spec or SPI communication. However, I would like to find out if any one has done similar design, and what's the distance they were able to acheive using SPI bus on 2812.
Thanks in advance.
Greg