This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TMS320F28379D: USB.lib

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

Tool/software: TI-RTOS

Good Day,

We have a project which uses both CAN and USB functionality. The libraries we have used are deprecated, and I have been tasked with updating the CAN functionality to the 1.0.03/1.0.04 versions. I have found during the process that this causes issues with the USB functionality, as several of the library calls still rely on deprecated code. The usb.lib file is making some calls to the older USB code, and this is giving me some trouble. My current thought is to update the calls and build a new library file, however I am unsure of how to determine what files this was built from. If possible, could you provide me with the contents (.c and .h) files that were used to build the USBlib.lib file found in C2000Ware_1_00_03_00\libraries\communications\usb\f2837xs\lib? Thank you for any assistance.