This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8312-69M-KIT: Need information for Development Board to Motor connection details

Part Number: DRV8312-69M-KIT
Other Parts Discussed in Thread: TMS320F28069M, DRV8312, CONTROLSUITE

Hi

I have DRV8312-69M-KIT-Three Phase BLDC Motor Kit with DRV8312 and InstaSPIN-Enabled Piccolo TMS320F28069M MCU

I see multiple wires connected to motors, which are not labeled.

Also could not find clear details in user guide, about which wires needs to be connected to which development board slots.

Since this is a motor, I am being extra careful.

Can anybody please provide/suggest detailed description motor and board connection details , with pictures would be really helpful.

Thanks

Rajarama

  • If you download and install the controlSUITE, you may find and refer to DRV8312-C2-KIT Hardware Reference Guide (DRV8312_C2_KIT_HWGuide.pdf ) in the folder of C2000 controlSUITE as below, there is a clear guide about how to connect the motor.

    \ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\~Docs.