Part Number: TMS320F28379D
Other Parts Discussed in Thread: TIDM-DELFINO-ETHERCAT, , CONTROLSUITE, TMDSCNCD28379D
Tool/software: Code Composer Studio
Hi, everyone.
I would like to test EtherCat on F28379D, and need to buy a fit board from TI.
I find two boards which are "TMDSECATCNCD379D" and "TIDM-DELFINO-ETHERCAT". Which one should i need to buy?
TMDSECATCNCD379D have the above picture . It is shown that there are two boards ,the ethercat ET110 on the adpter board and the TMS320F28379D on the control board .
It is enough only to buy TMDSECATCNCD379D .
Another board green is included in the above picture, It is used to supply the power and output all of pins from 28379d . do I need to buy it together?
Now in china , the board often use JTAG to debug which has 14pins . I have seed-XDS560V2(Arrow) tool to emulate dsp chip .Can I use this emulater on EtherCat solution, if not ,which type emulater should I buy, please give me the specific name and link .
I hope I do not need to buy power supply.
Thank you very much !
Best Regards!
Richie