Part Number: TMDSSOLARUINVKIT
The zero ohm resistor R202 blew up while conducting "Build 2: Inverter Closed Current Loop with GRID". I erroneously connected the AC socket to the Development board via J1 which led to R202 blowing up. The board is now not fully functional; once the 15V & 12V DC isolated biases are connected, LED 3 on the board is blinking and not continuous & LED 1 on the control card is OFF, therefore the control card cannot connect to CCS. Kindly advice on the procedure to fix the development board.
Do you have any recommendation on whom can fix the board?