This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Firmware upgrade using CAN

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE

Hi,

I wanted to update the firmware of an F28379D Launchpad using CAN bus. This will be done using a Cortex-M4 processor. I wanted to know if:

1.) Are the CAN based ROM bootloader source files available so that if any updates are required in the bootloader, I can make changes and use it as a flash based bootloader (since ROM based bootloader can not be overwritten).

2.) I know about the SCI flash kernels. How feasible is the porting of the SCI flash kernel to a CAN based kernel?

Regards,

Apoorv