Part Number: TMS320F280049
Other Parts Discussed in Thread: C2000WARE
Hi Champion,
I have two question about CAN CLK:
1. Baud rate = CAN clock / {[(BRP + 1)+(BRPE *64)]*(Tseg1 + Tseg2 + 1)}, so in CAN CTR register, Tseg1 = Tseg2 or Tseg1 + 1 = Tseg2 and TSJW = min(Tseg1 ,Tseg2, 4), right?
2. After test, no matter we config
ClkCfgRegs.CLKSRCCTL2.bit.CANBBCLKSEL = 0 or 1 CAN clock also same, for example 10MHz, but this bit is decide CAN clock source sysclk(100MHz) or crystal(10MHz), this two clk sorue is 10x gap, why CAN final clock is same?
Thanks!
BR
Joe