Part Number: TIDM-BLPFC
Tool/software: Code Composer Studio
the SCH is from controlSUITE\development_kits\BLPFC_v1.0\Hardware
the software is from controlSUITE\development_kits\BLPFC_v1.0
The channel 1 is intput voltage ,The channel 2 is intput current
When I use the build 3 to the BLPFC board ,the output voltage just keep in 250V not 385V.
VBUS_RATED_VOLTS is set 390V.
sometime the output voltage will get through 385V, at same time the Vcmd will get high too.the input distortion.
how can i do for this problem?