This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: Methods to override the internal pulls during reset

Part Number: TMS320F28069

1.Except PWM pins,the pullups on other GPIO pins are enabled upon reset.Can I change this default behaviour of the MCU.

2.What is the strong PD resistor value to override the internal pull up during reset.

  • Jagbir,

    1. You cannot change the default behavior.
    2. A pull down resistor depends on the application.
      1. If its going on TRSTn then 2.2Kohms is recommended to ensure absolutely no glitching occurs
      2. Other pins typically a 4.7K ohm resistor is recommended.

    Regards,
    Cody