Part Number: TMS320F28377S
while selecting the trigger sources for the trip inputs in Digital compare module, is it possible to select multiple trigger sources for the same trip input?
for example for TRIPIN4 in digital compare module there is a mux configuration to select the trigger sources, there are two registers TRIP4MUX0TO15CFG and TRIP4MUX16TO31CFG. and a register to enable the MUX (TRIP4MUXENABLE) . Can I use this register to enable multiple MUX modules just like below?
EPwmXbarRegs.TRIP4MUXENABLE.bit.MUX0 = 1;
EPwmXbarRegs.TRIP4MUXENABLE.bit.MUX6 = 1;
EPwmXbarRegs.TRIP4MUXENABLE.bit.MUX2 = 1;