Part Number: TMS320F28375D
Hi champs,
I have a question about EMIF2 16bit memory interface.
On TRM P.2612
-------------------------------------------------
The EMIF address pin EM1A[0] always provides the least significant bit of a 32-bit word address. Therefore, when interfacing to a 16-bit or 8-bit asynchronous device, the EM1BA[1] and EM1BA[0] pins provide the leastsignificant bits of the halfword or byte address, respectively.
-------------------------------------------------
This is for EMIF1.
When it uses EMIF2,
-------------------------------------------------
The EMIF address pin EM2A[0] always provides the least significant bit of a 32-bit word address. Therefore, when interfacing to a 16-bit or 8-bit asynchronous device, the EM2BA[1] and EM2BA[0] pins provide the leastsignificant bits of the halfword or byte address, respectively.
-------------------------------------------------
As above, is my understanding correct?
Does it work correctly when connected as follows?
Delfino Asynchronous
EM2A[0] ADR[0]
EM2A[1] ADR[1]
-
-
-
EM2A[12] ADR[12]
Regards,
Shinji Ueda