Part Number: TMS320F28375S
Other Parts Discussed in Thread: TMS320F2837
Hi,
I have one question regarding the usage of TRST pin in JTAG. Usually with other controllers to ensure complete hardware reset, TRST needs be asserted at power-up and whenever RESET is asserted (for ex: RESET issued from voltage supervisor is also fed into this). Do we need to do that in TMS320F2837 as well?
But the datasheet doesn't mention this explicitly. If this pin is LOW, device is functional & when driven HIGH, gives the scan system control of the operations (doesn't seem to be RESETing the JTAG TAP controller)
could anyone please help me with the TRST connection. should this be involved in RESET (or) I can pull it down with 2.2k all the time
Thanks in advance
Thanks & Regards
Muthu A