Other Parts Discussed in Thread: MOTORWARE, CONTROLSUITE
I need to caveat all of the following with "I've only just picked this up, so bear with my stupidity"...
Looking to find the quickest/simplest way to get to an absolute position control demonstration using the HV Eval box (TMDSHVMTRINSPIN), HV motor (HVBLDCMTR) and an SSI absolute encoder.
Q1: is there anything built into the eval software which will enable absolute position controlling?
Q2: does the eval kit support the insertion of an SSI-interfaced absolute encoder?
Q3: can anyone recommend a fast solution to getting position control operational?
Apologies for the strange tack: although I'm personally sold on using Instaspin technologies, I need to convince some non-technical people this is the way forward: simplest way to do this is to have a motor running in front of them!
cheers
Mat