Part Number: TMDSDC3359
Other Parts Discussed in Thread: UNIFLASH
Hello,
We've bought a TMDSDC3359 (revD) and we are trying to flash the G3 DC firmware using PLC_setup.sh tool but without sucess.
We have connected the PLC SOM to it's P2 connector and powered the board with the 12VDC source.
Here is the command output:
.##################################################### # Flashing Data Concentrator with G3 standard #===================================================== # Script will run the following command: # /home/root/PLC/util/dspFu -c /dev/ttyO3 -f /home/root/PLC/G3_DC/sysbios_g3_plc_dc_F2806x_AFE031_CRC16_MSB.sbin '##################################################### Opening file - /home/root/PLC/G3_DC/sysbios_g3_plc_dc_F2806x_AFE031_CRC16_MSB.sbin Image format - BINARY Image file size - 137040 bytes Serial device - /dev/ttyO3 Setting host and diag port to SCI-A .... No response from DSP !! - exiting !! .===========================================================. | ERROR: Firmware upgrade failed | |===========================================================| | Suggestions to fix issue: | | - Verify PLC SOM is securely attached to EVM | | - Make sure PLC SOM was pre-flashed with hex image | '===========================================================' Press ENTER key to return back to main menu
We tried to detect the Zero Configuration GUI using the rs232 on top but still no serial communication.
Please what are the proper steps to flash G3 DC firmware in the PLC SOM ?
BR,
Kamel B.