Part Number: TMS320F28379D
Tool/software: TI C/C++ Compiler
My program is in C++ (all my sources have .cpp) and I use the -cpp_default option to compile the device specific C files using CCS V7 using CL2000 version 16.9.x . I am able to link and flash successfully, however it does NOT survive a power reset. furthermore the EQEP register values are not what was expected. While program runs, I am able to debug through CCS.
On a second note I wrote the same program in C (linked against the same device files) and that seems to work fine including EQEP updates. I am using the same linker command across C and C++ builds.
The working C program when compiled with -cpp_default does not work correctly and the flash does not survive power reset.
I would really like to debug the C++ version, any pointers appreciated on how to debug this.Thanks.