Part Number: TMDSILPFCKIT
Hi,
I have bought TMDSILPFCKIT, I was wondering if the Eval-board is also compatible with F28335 control card?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSILPFCKIT
Hi,
I have bought TMDSILPFCKIT, I was wondering if the Eval-board is also compatible with F28335 control card?
Thanks,
This eval-board runs only with F28035 control card. The CCS project does not include F28335 code. So if you want to use F28335 control card, you have to develop the code and validate it.
Shamim
Dear Shamim,
Thanks for your response. So if I understood correctly, I can use F28335 on this eval board but I have to code it myself?
You mean that the GUI interface designed for this eval board is only for F28035 control card right?
Best regards,
Pooya
Yes, you have to code it yourself for F28335.
Our code is valid only for F28035. You can use any other MCU, but you need to develop the code or change the code accordingly.
Shamim