This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Program and Data size About 28335_RAM_lnk.cmd.

hi,~ i need yours help  in based  ram mode.

 MEMORY
{
PAGE 0 :
   BEGIN      : origin = 0x000000, length = 0x000002     /* Boot to M0 will go here                      */
   RAMM0      : origin = 0x000050, length = 0x0003B0
  
   RAML0      : origin = 0x008000, length = 0x004000
   ZONE7A     : origin = 0x200002, length = 0x00FC00    /* XINTF zone 7 - program space */
   CSM_RSVD   : origin = 0x33FF80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
   CSM_PWL    : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA            */
   ADC_CAL    : origin = 0x380080, length = 0x000009
   RESET      : origin = 0x3FFFC0, length = 0x000002
   IQTABLES   : origin = 0x3FE000, length = 0x000b50
   IQTABLES2  : origin = 0x3FEB50, length = 0x00008c
   FPUTABLES  : origin = 0x3FEBDC, length = 0x0006A0
   BOOTROM    : origin = 0x3FF27C, length = 0x000D44   

PAGE 1 :
   BOOT_RSVD  : origin = 0x000002, length = 0x00004E     /* Part of M0, BOOT rom will use this for stack */
   RAMM1      : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAML4      : origin = 0x00C000, length = 0x004000
   ZONE7B     : origin = 0x20FC00, length = 0x000400     /* XINTF zone 7 - data space */
}

section{

.text :> RAML0      .ebss:>RAML4       }

Upper is my .cmd file.  I  spending 0x4000(in text) and 0x4000(in ebss) . Program  and data are size totoal  32k.  I kenw that 28335 basic  ram size is 68k

I need a more than program and data size. BUT BUT  when I bigger size there are error event. i doen`t konw why? Actually resting 36k.

whitch part  was controled  size ??    I need a 0x006000(in text) and 0x006000(.ebss) whitout XINTF. How to solve this problem. piz heip me.~~