This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TIDM-HV-1PH-DCAC: problem with starting "Build 2_DEMO"

Part Number: TIDM-HV-1PH-DCAC
Other Parts Discussed in Thread: TIEVM-HV-1PH-DCAC

Tool/software: Code Composer Studio

hello i have some trouble with "TIEVM-HV-1PH-DCAC"

1) There was a problem during the "3.1.2.3.4.3 running the code" session of the  "User Guide(TIEVM-HV-1PH-DCAC, grid connected)

2) <Capture#1> is the screen of the Build2_DEMO after clicking "run the project".


<capture#1>
3) <Capture#2> is after the voltage of AC supply is set to 110V / 60Hz.

<capture#2>
4) After that, I slowly raised the voltage of the DC supply. However, when the DC voltage reaches 190, the click of the relay is heard and it is shown as <Capture#3>.

<capture#3>


5) At the same time, the AC supply is put into the fault state by the protection program.

what is wrong with this?


PS,

 when i run the project and continuous refresh it, Scriptconsol show me boardstatus_Overcurrenttrip

i knew when i progress the project it change to boardstates_NoFault

but is it OK?