This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: Possible To Route Scaled Signal From eCap to HRCAP?

Part Number: TMS320F28069

Hello TI,

I see this was never answered.

Would be handy if possible.

Thanks,
John W.

  • John,

    on this device(F280069) the eCAP and HRCAP modules are completely independent and therefore they share no resources. So no this cannot be done.

    On newer devices using a Type-1 eCAP module the HRCAP has been integrated into the eCAP, however the event prescaler is not available when using the HRCAP enhancements. This is because he event prescaler  is synchronized to SYSCLK, rendering the HRCAP enhancements useless.

    Stated another way: The HRCAP's only advantage over the eCAP is that it can measure signals that are a fractional portion of a SYSCLK, if you synchronize a signal to SYSCLK first, then take a measurement, you have eliminated the benefit of the HRCAP.

    Regards,
    Cody 

  • Cody,

    OK - thanks,
    John