Part Number: TMS320F2809
We are cold soaking a ups to -10C. The processor will start up breiefly then the xrs pin goes low for a few hundred milliseconds then high for 1.5 seconds then low then repeat. The input supplies look good during this time so they have been ruled out. there is a 10k pullup on the xrs pin with a 1n cap to gnd. We do not have the watchdog timer enabled in the firmware so we fail to see how the DSP is able to pull the xrs pin low. Once we let the unit warm up a few degrees it does start normally.
Can the xrs pin be pulled low by other means. As I said the watchdog timer is not enabled.
Thanks!