Part Number: TMDSSOLARUINVKIT
Tool/software: Code Composer Studio
Hi,
I am looking over the reference design "TMDSSOLARUINVKIT" and have following question.
- The key highlights of the output power is 280W@220Vac/140W@110Vac; however, there is only one DC-DC Flyback stuffing on the "TMDSSOLARUINVKIT". Does it mean that one DC-DC Flyback can deliver 280W or two DC-DC Flybacks are necessary to support 280W power output? Does the current software support two DC-DC Flybacks?
Thanks.