This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: MCU abnormity process

Part Number: TMS320F28335

Hi TI,

We add abnormity check procedure in our software such as checking broken RAM,broken ROM and so on.So we should add some extra procedure to do abnormity process when there is abnormity to make the MCU be on controllable state reducing dangerous output.Can you give me some advisable suggestion to solve this problem that what the MCU should execute ?

Best regards,

Frank

  • Hi Frank,

    There is a IEC 60730 Diagnostic Library available for the F2833x device. There is a March13n algorithm in the software package which tests for RAM failures.

    www.ti.com/.../iec60730swpackages

    Regards,
    sal
  • If a failure is identified and it is a dangerous fault, it is up to you to handle the failure and either repair it if possible or go to a safe state.

    sal
  • Hi Sal,
    Thanks.It is said there is a way that MCU calls the function 'assert()' when there is a error ,I don't know which state the MCU be on after call the function,is that in debug mode or other?By the way,if there is a watchdog used in the application,what we should do when errors occur?MCU should fed the watchdog not to call assert() rather than?
    Best regards,
    Frank
  • The asserts should only be compiled in a debug build configuration. You are free to use it and supply the function which is called if the assert fails.

    The assert is likely only for software systematic errors. For example passing the wrong parameter to a function. I do not believe the assert function is called on a hardware error. You can confirm.

    If you detect a fault, it is up to you to feed the watchdog while you take the system to a safe state, or you can not feed the watchdog and cause a watchdog reset as long as you can ensure that the reset will not create a dangerous state in the system.

    Regards,
    sal