Other Parts Discussed in Thread: SFRA
Hi,
My application requires input voltage of 650VDC, power rating of 1.1kVA with output voltage options similar to that in the existing design. Please advise the design changes other than change in IGBT and gate drivers to scale up the design to suit my requirements.
If you can recommend a reference design for a simple 650VDC, 1.1kVA to 110V, 60Hz or 230V, 50Hz inverter with sine PWM control, it will be very helpful.
Regards,
Lakshmi