Part Number: TMS320F28379D
Other Parts Discussed in Thread: CONTROLSUITE
Hi,
Related to my previous question about transmitting the result of the adc to a hyperterminal via SCI which I managed to transmit the result correctly. Now I want to save the AdcResult to text file to be used later for further processing. what I added so far to my amended "adc_soc_epwm_cpu01.c" example are:
1- I defined a file Globally as (FILE *myFile).
2- In the Adca1_isr below I created a condition to open and close the file.
3- I tried to save a simple counter to the file using the fprintf function which resulted in that the alocated RAM for .text is not enough. SO I tried to change the .text ram alocation as following:
//.text : >>RAMM0 | RAMD0| RAMLS0, PAGE = 0 // I chaged it to this previously so that sprintf to work and it worked correctly.
.text : >>RAMGS12 | RAMGS13| RAMGS14| RAMGS15, PAGE = 1 // I chaged the above line to this line so that the fprintf works.
but when I did this change, the error which showed below is no more exist. HOWEVER, when I debug and run the project, the adcaResults buffer didn't receive and conversion results.
"C:/ti/controlSUITE/device_support/F2837xD/v210/F2837xD_common/cmd/2837xD_RAM_lnk_cpu1.cmd", line 54: error #10099-D: program will not fit into available memory. placement with
alignment/blocking fails for section ".text" size 0x2b3f page 0. Available memory ranges:
RAMM0 size: 0x2de unused: 0x1 max hole: 0x1
RAMD0 size: 0x800 unused: 0x0 max hole: 0x0
RAMLS0 size: 0x2000 unused: 0x1 max hole: 0x1
error #10010: errors encountered during linking; "adc_soc_epwm_cpu01.out" not built.
See my RAM file at the end of the post.
----------------------------------------------------------------------------------------------------------------------------------------------------
//
// adca1_isr - Read ADC Buffer in ISR
//
interrupt void adca1_isr(void)
{
AdcaResults[resultsIndex++] =AdcaResultRegs.ADCRESULT0;
if(RESULTS_BUFFER_SIZE == resultsIndex)
{
for (z=0;z<RESULTS_BUFFER_SIZE;z++)
{
Vin = AdcaResults[z];
send_result(Vin);
}
}
int counter = 0;
if (counter < 9){
myFile = fopen("AdcaResults.txt","w");
fprintf(myFile,"%d\n",counter);
//printf(filePtr,"%d,",AdcaResults);
counter++;
}
else if(counter == 9){
fclose(myFile);
}
if(RESULTS_BUFFER_SIZE <= resultsIndex)
{
resultsIndex = 0;
bufferFull = 1;
}
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
-------------------------------------------------------------------------------------------------------------------------------------------------------
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE // length was = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x002000 // this was 0x000800
// RAMLS1 : origin = 0x008800, length = 0x000800 // was 0x000800
// RAMLS2 : origin = 0x009000, length = 0x000800 // was 0x000800
// RAMLS3 : origin = 0x009800, length = 0x000800 // was 0x000800
// RAMLS4 : origin = 0x00A000, length = 0x000800 // was 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x001000
RAMGS3 : origin = 0x00F000, length = 0x001000
RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
RAMGS12 : origin = 0x018000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS13 : origin = 0x019000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS14 : origin = 0x01A000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS15 : origin = 0x01B000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
CANA_MSG_RAM : origin = 0x049000, length = 0x000800
CANB_MSG_RAM : origin = 0x04B000, length = 0x000800
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0
// .text : >>RAMM0 | RAMD0 | RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4, PAGE = 0
//.text : >>RAMM0 | RAMD0| RAMLS0, PAGE = 0 // I chaged the above line to this line
.text : >>RAMGS12 | RAMGS13| RAMGS14| RAMGS15, PAGE = 1 // I chaged the above line to this line so that fprintf works
.cinit : > RAMM0, PAGE = 0
.pinit : > RAMM0, PAGE = 0
.switch : > RAMM0, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.cio : > RAMGS15, PAGE = 1 // I added this Line, was not here
.stack : > RAMM1, PAGE = 1
.ebss : > RAMGS13, PAGE = 1 // was RAMLS5 I changed to open text file
.econst : > RAMGS14, PAGE = 1 // was RAMLS5
.esysmem : > RAMLS5, PAGE = 1
Filter_RegsFile : > RAMGS0, PAGE = 1
ramgs0 : > RAMGS0, PAGE = 1
ramgs1 : > RAMGS1, PAGE = 1
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} > RAMM0, PAGE = 0
#else
ramfuncs : > RAMM0 PAGE = 0
#endif
#endif
/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
/* The following section definition are for SDFM examples */
Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
Difference_RegsFile : >RAMGS5, PAGE = 1, fill=0x3333
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
kind Regards
Hayder