Part Number: TIDM-HV-1PH-DCAC
Other Parts Discussed in Thread: TIEVM-HV-1PH-DCAC
Tool/software: Code Composer Studio
hello
When I use "TIEVM-HV-1PH-DCAC" I`m get in trouble,
the input sensor of inverter was not work (guiVbus)
It was "Build 2 : DEMO". when I raise DC source to 190V I can`t realized the boardstate was tripped by overcurrenttrip.
then I raised DC source to 380V, I thought it was broken at that time.
from then, it can`t sense the Voltage.
What should I do?
was the sensor broken? or was there another reason?
How can I fix it?
PS. when I check it to “Build 1 : open loop” despite the increased voltage, the input sensor was move like Fig 1. looks like just ripple
<Fig 1>