Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: C2000WARE, TMS320F28069, DRV8305
Tool/software: Code Composer Studio
Hi,
Trying out the Example_2806xGpioToggle.c with a LAUNCHXL-F28069M V1.2 located in
C2000Ware_1_00_02_00\device_support\f2806x\examples\c28\gpio_toggle
with CCS Version: 8.0.0.00016, I get this error, when I try to
Run->Load->Example_2806xGpioToggle
"C28xx: Error connecting to the target: (Error -1135 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 7.0.188.0) "
AFAICS, the debug connections are on the Launchpad itself, so likely no issue in the connections. I dont see how it is possible to reset the probe either.
Any idea, why the probe seem unable to connect to the F28069 ?
Thanks,
Manu