Part Number: TMS320F28027
Other Parts Discussed in Thread: LAUNCHXL-F28027
Hello,
I have a question.
I am running my custom project on LAUNCHXL-F28027 with external clock input to GPIO19.
But I'm facing following errors.
Can't Single Step Target Program:
(Error -1156 @ 0x800)
Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device.
(Emulation package 6.0.407.3)
C28xx: Failed CPU Reset
C28xx: Error occurred during flash operation: CPU Reset error. Error code 1
Could you tell me how to solve this problem?
Regards,
U-SK