Part Number: TMS320F28377S
Tool/software: Code Composer Studio
Hi guys.
I saw a bunch of questions and answers, but none of the answer what is happening here.
In the 28335 i always calculeted the EPWM_TIMER_TBPRD like :
EPWM_TIMER_TBPRD = 150 Mhz / (2 * SwitchingFreq) For exemple (SwitchingFreq = 12Khz) = 150 Mhz / (2 * 12k) = 6250 for UpDown
But for the 28377 i saw that the Epwm for it is half of the clock - Meaning 100 Mhz, thus EPWM_TIMER_TBPRD should be like:
EPWM_TIMER_TBPRD = 100 Mhz / (2 * SwitchingFreq) For exemple (SwitchingFreq = 10Khz) = 100 Mhz / (2 * 10k) = 5000 for UpDown
however i need to set 2500 to get 10kHz.
and i am using the Epwm configured like this:
EPwm6Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm6Regs.TBCTL.bit.CLKDIV = TB_DIV1;
Thanks guys !