Part Number: TMS320F28335
Tool/software: Code Composer Studio
Good morning,
i m using a TMS320F28335 and i need some information.
I have necessity tu flash the device and i try FlashBurn4.1. But the connection fails.
I have tried to verify the connection by means of CCS, but connection fails.
I have problem (test Connection) to connect to TMS320F28335 with BH-USB-200 and CCS5.5.
i want to ask if there are problems using BH-USB-200 and CCS5.5? are there particular configuration to make?
Connection to board with CCS5.5 by means of BH-USB-2000 Test Connection work properly. (it was necessary to change the sense to FALLING edge). With BH-USB-200 CONNECTION Fail.
Can you suggest some test to try?
Thanks in advance.
Fabio