Part Number: TMS320F28335
I am having difficulties while running a simulink model in my DSP.
1) The model runs with no errors on normal mode, but but when I set it to run on external mode, it shows different signals from the original ones. The figures are attached.
2) When trying to run it from the flash memmory, I get the old error "Error occurred while executing External Mode MEX-file 'ext_comm':
Failed to connect to the target. A time-out occurred while waiting for the connection response from the target. Possible reasons for the time-out:
a) The target is not switched on.
b) The target is not connected to your host machine.
c) The application for the model is not running on the target. You might have clicked the Stop button. If the Run button is not dimmed, click it. Otherwise, click the Build button, which downloads and runs your application on the target."
Which parameter could cause that?