Part Number: TMS320F28035
Hi Friends,
I'm working with I2C EEPROM (AT24C04), for that I've imported sample code from control-suit.
Sample code works fine only if I write 2 or 4 bytes of data and again read back from EEPROM,
but as I change followings;
#define I2C_MAX_BUFFER_SIZE 6//2
#define I2C_NUMBYTES 8 //4
MsgBuffer [ I2C_NUMBYTES ] with 6 bytes of data
Reading from EEPROM address register can't be executed.
FYI: I've observed into watch window that Register Ready Access Interrupt Flag is not generated, I didn't modify the sample code, except for the above mention 2 lines and buffer of 6 bytes